Solid Edge Framework Type Library
SeekWriteAccess Method
Returns true if write access is available and false if it is not available.
Description
Seeks write access to the document if it is available.
Syntax
Visual Basic
Public Sub SeekWriteAccess( _
   ByRef WriteAccess As Boolean _
) 
Parameters
WriteAccess
Returns true if write access is available and false if it is not available.
See Also

SolidEdgeDocument Object  | SolidEdgeDocument Members

Send comments on this topic.