|  AlternatePath | Sets and returns an alternate path to access the source file for the referenced Symbol2d object. | 
|  Angle | Sets and returns the angular rotation of the referenced object. | 
|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Class | Returns the class description of the source document for the referenced Symbol2d object. | 
|  ContentsLocatable | Specifies whether or not the referenced Symbol2d object's contents can be located. | 
|  DisplayType | Sets and returns the display type for the referenced object. | 
|  Document | Returns the document to which the referenced object belongs. | 
|  Index | Returns the numeric index for the active object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Key | Returns a key (a string) to find the object relative to its owning parents. | 
|  KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. | 
|  Layer | Sets and returns the named layer on which the referenced object resides. | 
|  MemberReference | Creates an object that refers to the specified object in the context of the symbol occurrence | 
|  Name | Returns the name of the referenced object. | 
|  NestedDisplay | Sets and returns the placeholder display behavior when the associated attachment is nested. | 
|  Object | Returns the dispatch interface associated with the site. | 
|  ObjectVerbsCount | Gets the number of verbs supported by an object. | 
|  OLEType | Returns the insertion type for the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Quantity | Sets and returns the number of occurrences of an object. | 
|  ScaleFactor | Sets and returns the scale factor between an object and its source document. | 
|  ScaleFactorLock | Specifies whether or not the scale factor of the referenced Symbol2d object is locked. | 
|  SourceDoc | Returns the file name of the document used as a template for the referenced object. | 
|  SourceDocument | Returns the embedded or linked Draft document. | 
|  Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. | 
|  Type | Specifies the type of the object being referenced. | 
|  UpdateOptions | Sets and returns the update status of an OLE object when the source is modified. | 
|  User | Returns the user attribute set for the referenced Symbol2d object. | 
|  UseSymbolLayer | Sets and returns the Use_Symbol_Layer flag for the referenced Symbol2d object. | 
|  ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |