Solid Edge Framework Type Library
Angle Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
Symbol2d Object
: Angle Property
Description
Sets and returns the angular rotation of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Angle As Double
Remarks
For Rectangles, this value represents the rotation of the entire object. The angle is represented in Radians.
See Also
Symbol2d Object
|
Symbol2d Members
Send comments
on this topic.