Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Caption | Sets and returns the caption of the referenced object. |
DrawHwnd | |
Environment | Returns the Environment object for the referenced Window object. |
Height | Returns the height of the referenced object. |
hWnd | Returns the window handle for the referenced object. |
Icon | Returns the collapse icon handle (HICON) for the referenced Window object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Left | Specifies the distance (in twips) between the internal left edge of an object and the left edge of its container. |
Parent | Returns the parent object for the referenced object. |
SelectSet | Returns the current selection set for the referenced document. |
Top | Sets and returns the distance from the top of the screen to the top of the referenced object or control. |
Type | Specifies the type of the object being referenced. |
UsableHeight | Returns the height of the usable vertical space in the application window. |
UsableWidth | Returns the width of the usable horizontal space in the application window area. |
View | Returns the View object for the referenced Window ojbect. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
Width | Returns the width of the referenced object. |
WindowNumber | Returns the window number of the referenced Window object. |
WindowState | Returns or sets the state of the referenced window. |