Solid Edge Framework Type Library
Top Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
Window Object
: Top Property
Description
Sets and returns the distance from the top of the screen to the top of the referenced object or control.
Property type
Read-write property
Syntax
Visual Basic
Public Property Top As Integer
Remarks
Sets and returns the distance from the top edge of the physical screen to the top edge of the main application window, in points (1/72 inch).
See Also
Window Object
|
Window Members
Send comments
on this topic.