|  Application | Returns the active application object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by the specified vector. | 
|  FacetCount | Returns the number of facets on the referenced object. | 
|  GeometryForm | Specifies the geometry form of the referenced object. | 
|  IsOverriddenBody |  | 
|  IsSolid | Indicates whether or not the referenced object encloses a finite, well-defined volume. | 
|  Loops | Returns the set of loops in the Body. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Shells | Returns a Shells collection object. | 
|  Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. | 
|  Tag | Returns the Tag of the Body. | 
|  Type | Returns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object. | 
|  UpdatesCounter | Returns the number of times the referenced object has been modified. | 
|  Valid | Indicates whether or not the body passes topological and geometric checks. | 
|  Vertices | Returns the set of vertices in the Body. | 
|  Visible | Controls the display of the referenced object. | 
|  Volume | Indicates the volume of the referenced object in cubic meters. |