Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBody As SolidEdgeGeometry.Body
    Dim dblDensity As Double, dblAccuracy As Double, dblVolume As Double
    Dim dblArea As Double, dblMass As Double, dblCGravity(1 To 3) As Double
    Dim dblCVolume(1 To 3) As Double, dblGMomInertia(1 To 6) As Double, dblPMomInertia(1 To 3) As Double
    Dim dblPrinAxes(1 To 9) As Double, dblRadGyration(1 To 3) As Double, dblRAccAchieved As Double
    Dim lngStat As Long
    Const TESTFILE = "T:\vbtests\testcases\cube.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the body object of the model
    Set objBody = objDoc.Models(1).Body
    ' getting the PhysicalProperties collection for the Body object
    dblDensity = 1
    dblAccuracy = 0.001
    Call objBody.ComputePhysicalProperties(Density:=dblDensity, Accuracy:=dblAccuracy, _
                                           Volume:=dblVolume, Area:=dblArea, Mass:=dblMass, CenterOfGravity:=dblCGravity, _
                                           CenterOfVolume:=dblCVolume, GlobalMomentsOfInteria:=dblGMomInertia, _
                                           PrincipalMomentsOfInteria:=dblPMomInertia, PrincipalAxes:=dblPrinAxes, _
                                           RadiiOfGyration:=dblRadGyration, RelativeAccuracyAchieved:=dblRAccAchieved, Status:=lngStat)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
End Sub