Solid Edge Geometry Type Library
Vertex Object
Members
Collapse All
Expand All
Solid Edge Geometry Type Library
: Vertex Object
Description
Holds the topological position of the endpoint of an Edge.
Remarks
More than one edge can terminate at this same point. This object holds the relationship to all such edges.
See Also
Vertex Members
Send comments
on this topic.