|  Application | Returns the active application object. | 
|  Body | Returns the Body of the Vertex. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  ID | Returns the Parasolid ID of the Vertex. | 
|  Loops | Returns the Loops that are bounded by the current Vertex. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Shells | Returns the shells that are bounded by the current Vertex. | 
|  Tag | Returns the Tag of the Vertex. | 
|  Type | Returns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object. | 
|  UpdatesCounter | Returns the number of times the referenced object has been modified. |