Solid Edge Framework Type Library
MatTable Object Members
Overview 
Public Methods
Public Method AddCustomProperty
Public Method AddMaterialAdds material to material table.
Public Method AddMaterialToFavorites
Public Method AddMaterialToLibrary
Public Method ApplyMaterial
Public Method ApplyMaterialToDoc
Public Method ClearMRUList
Public Method CreateNewDirectory
Public Method CreateNewMaterialLibrary
Public Method DeleteCustomProperty
Public Method DeleteMaterial
Public Method DeleteMaterialFromLibrary
Public Method EditOpenGageExcelFileThis method is used to open the Gage file for editing.
Public Method ExportMaterialDataToFile
Public Method GetCountOfCustomProperties
Public Method GetCurrentGageNameThis method is used to fetch the name of currently applied gage of a sheet metal document.
Public Method GetCurrentMaterialNameThis method is used to fetch the name of currently applied material of a sheet metal document.
Public Method GetCustomMaterialPropertyFromDoc
Public Method GetCustomMaterialPropertyFromLibrary
Public Method GetDefaultGageFileNameThis method is used to get the complete path of the gage excel file.
Public Method GetFavoriteMaterialList
Public Method GetMaterialLibraryFileList
Public Method GetMaterialList
Public Method GetMaterialListFromLibrary
Public Method GetMaterialPropValueFromDoc
Public Method GetMaterialPropValueFromLibrary
Public Method GetMaterialsFolderPath
Public Method GetMatLibFileName
Public Method GetMatPropValue
Public Method GetMRUMaterialLimit
Public Method GetMRUMaterialList
Public Method GetPSMGaugeInfoForDocThis API is used to get all the gage related information from a sheet metal document.
Public Method GetPSMGaugeListFromExcelThis method is used to obtain list of Gages from a Gage table.
Public Method ImportMaterialDataFromFile
Public Method PerformGageDataValidationThis method is used to validate a Gage for data integrity.
Public Method RenameDirectory
Public Method RenameLibrary
Public Method RenameMaterial
Public Method SetActiveDocument
Public Method SetDocumentToGageTableAssociationThis method will create an association between the sheet metal file and the Gage table.
Public Method SetMaterialPropValueToLibrary
Public Method SetMaterialToGageTableAssociationThis method is used to create an association between a material and a Gage table.
Public Method SetMatPropValue
Public Method SetMRUMaterialLimit
Public Method UseNeutralFactorFromExcelThis method is used to decide source of the Neutral Factor.
Public Method WriteMaterialDataToXML
Public Method WriteMatLibFileFromXML
See Also

MatTable Object  | Solid Edge V17 - What's New