| Solid Edge Framework Type Library > SolidEdgeInsightXT Object : CheckInDocumentsToInsightXTServer Method |
A Boolean flag. It has following possible values:
| Visual Basic |
|---|
Public Sub CheckInDocumentsToInsightXTServer( _ ByRef ppsaFileList() As Variant, _ ByVal bOnlyUpload As Boolean, _ ByVal bstrURL As String _ ) |
A Boolean flag. It has following possible values:
For checking in the documents checked out by the user from the InsightXT server. User can pass multiple files to be Checkin/Upload at a single time. The API also honors the ‘DisplayAlerts’ flag. If the flag is TRUE then Upload dialog will be shown while uploading and if the flag is FALSE then the dialog will not show.
![]() |
The case in which if the display_alerts flag is off and the CPD dialog is suppressed, then it is the responsibility of the caller to put the item id/item rev correctly into the file storage. He can use the API AssignItemID to assign the item id/item rev. If the document which is going to be uploaded is without item-id in the document number field then the value of the hr will be returned as E_INVALIDARG. |
Private Sub Command1_Click() On Error Resume Next Dim objApplication As SolidEdgeFramework.Application Dim objSolidEdgeInsightXT As SolidEdgeFramework.SolidEdgeInsightXT Set objApplication = GetObject(, "SolidEdge.Application") Set objSolidEdgeInsightXT = objApplication.SolidEdgeInsightXT Dim varInputList(1) As Variant varInputList(0) = "F:\010088.par" varInputList(1) = "F:\010087.par" Dim bOnlyUpload As Boolean bOnlyUpload = False Call objSolidEdgeInsightXT.CheckInDocumentsToInsightXTServer(varInputList, bOnlyUpload) Set objSolidEdgeInsightXT = Nothing Set objApplication = Nothing End Sub