Solid Edge Part Type Library
Index Property
Description
Returns the numeric index for the active object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Index As Long
Remarks
This index is the sequence that the object holds in its collection object (as held by the parent).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objHols As SolidEdgePart.Holes2d
    Dim objHol2d As SolidEdgePart.Hole2d
    Dim objProfile As SolidEdgePart.Profile
    Dim lngIdx As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create a Holes2d collection object
    Set objHols = objProfile.Holes2d
    ' Create a Hole2d object
    Set objHol2d = objHols.Add(xCenter:=0, yCenter:=0)
    ' Get the Index of the Hole object
    lngIdx = objHol2d.Index
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objHols = Nothing
    Set objHol2d = Nothing
    Set objProfile = Nothing
End Sub
See Also

Hole2d Object  | Hole2d Members