Solid Edge Part Type Library
SetCenterPoint Method
Specifies the x coordinate for the new center point.
Specifies the y coordinate of the new center point.
Description
Relocates the center point of the specified object.
Syntax
Visual Basic
Public Sub SetCenterPoint( _
   ByVal x As Double, _
   ByVal y As Double _
) 
Parameters
x
Specifies the x coordinate for the new center point.
y
Specifies the y coordinate of the new center point.
Remarks
The new center point is specified in x and y coordinates. As a result of the SetCenterPoint method, the object is repositioned with respect to the new center point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objHols As SolidEdgePart.Holes2d
    Dim objHol2d As SolidEdgePart.Hole2d
    Dim objProfile As SolidEdgePart.Profile
    Dim x As Double, y As Double
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create a Holes2d collection object
    Set objHols = objProfile.Holes2d
    ' Create a Hole2d object
    Set objHol2d = objHols.Add(xCenter:=0, yCenter:=0)
    ' Set the CenterPoint of the Hole
    Call objHol2d.SetCenterPoint(x:=0.1, y:=0)
    ' Get the CenterPoint of the Hole
    Call objHol2d.GetCenterPoint(x:=x, y:=y)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objHols = Nothing
    Set objHol2d = Nothing
    Set objProfile = Nothing
End Sub
See Also

Hole2d Object  | Hole2d Members