Add2dModelView | This method creates a 2D Model view as a DrawingView object. |
AddAssemblyView | Adds an assembly drawing view based on the ViewType and an optional configuration name. |
AddByAuxiliaryFold | Creates an auxiliary DrawingView object and a ViewPlane object from an existing DrawingView object. |
AddByDetailEnvelope | Creates an detail DrawingView object and a DetailEnvelope object from an existing DrawingView object. |
AddByDraftView | Adds a draft view that references the same user graphics as the input draft view. |
AddByFold | Creates a folded DrawingView object from an existing DrawingView object. |
AddDetailView | Creates an detail DrawingView object and a DetailEnvelope object from an existing DrawingView object. |
AddDraftView | Adds a scalable draft view to contain only user graphics. |
AddEmptyView | Adds an new empty, out-of-date drawing view. Specify parameters using view properties and then call Update. |
AddPartView | Adds a part drawing view based on the ViewType. |
AddPMIModelView | Adds an drawing view based on the specified PMI model view. |
AddSheetMetalView | Adds a sheet metal drawing view based on the ViewType. |
AddWeldmentView | Adds a weldment drawing view based on the ViewType. |
Align | Aligns selected principal and/or auxiliary DrawingView objects that are contained in a selection set. |
Item | The items in a collection. |
Unalign | Removes the alignment relationship between selected principal and/or auxiliary DrawingView objects that are contained in a selection set. |