Solid Edge Draft Type Library > DrawingViews Collection : AddAssemblyView Method |
Visual Basic |
---|
Public Function AddAssemblyView( _ ByVal From As ModelLink, _ ByVal Orientation As ViewOrientationConstants, _ ByVal Scale As Double, _ ByVal x As Double, _ ByVal y As Double, _ ByVal ViewType As AssemblyDrawingViewTypeConstants, _ Optional ByVal ConfigurationName As String, _ Optional ByVal Snapshot As Boolean = False, _ Optional ByVal SnapShotQuality As Long = 0 _ ) As DrawingView |
Value | Description |
---|---|
igBackView | View Orientation - Back View |
igBottomBackLeftView | View Orientation - Bottom Back Left View |
igBottomBackRightView | View Orientation - Bottom Back Right View |
igBottomFrontLeftView | View Orientation - Bottom Front Left View |
igBottomFrontRightView | View Orientation - Bottom Front Right View |
igBottomView | View Orientation - Bottom View |
igDimetricBottomBackLeftView | |
igDimetricBottomBackRightView | |
igDimetricBottomFrontLeftView | |
igDimetricBottomFrontRightView | |
igDimetricTopBackLeftView | |
igDimetricTopBackRightView | |
igDimetricTopFrontLeftView | |
igDimetricTopFrontRightView | |
igFrontView | View Orientation - Front View |
igLeftView | View Orientation - Left View |
igRightView | View Orientation - Right View |
igTopBackLeftView | View Orientation - Top Back Left View |
igTopBackRightView | View Orientation - Top Back Right View |
igTopFrontLeftView | View Orientation - Top Front Left View |
igTopFrontRightView | View Orientation - Top Front Right View |
igTopView | View Orientation - Top View |
igTrimetricBottomBackLeftView | |
igTrimetricBottomBackRightView | |
igTrimetricBottomFrontLeftView | |
igTrimetricBottomFrontRightView | |
igTrimetricTopBackLeftView | |
igTrimetricTopBackRightView | |
igTrimetricTopFrontLeftView | |
igTrimetricTopFrontRightView |
Value | Description |
---|---|
seAssemblyConfigurationSimplifiedView | Assembly Configuration Simplified Drawing View Type - This is a view of an assembly with simplification. The display of the simplified parts will be based on the configuration. |
seAssemblyDesignedView | Assembly Designed Drawing View Type - This is a view of an assembly with no simplification. |
seAssemblySimplifiedView | Assembly Simplified Drawing View Type - This is a view of an assembly with simplification. All parts in the assembly that have simplification will be displayed as simplified. |