Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCenterLines As SolidEdgeFrameworkSupport.CenterLines
    Dim objCenterLine As SolidEdgeFrameworkSupport.CenterLine
    Dim dblX As Double, dblY As Double, dblZ As Double
    Dim cHndType As HandleType
    Dim cKPType As KeyPointType
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Get the CenterLines object on the active sheet
    Set objCenterLines = objSheet.CenterLines
    ' Draw a CenterLine on the active sheet
    Set objCenterLine = objCenterLines.Add(x1:=0.25, y1:=0.15, z1:=0, _
                                           x2:=0.25, y2:=0.35, z2:=0)
    ' Get a KeyPoint
    Call objCenterLine.GetKeyPoint(Index:=1, x:=dblX, y:=dblY, z:=dblZ, _
                                   KeyPointType:=cKPType, HandleType:=cHndType)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCenterLines = Nothing
    Set objCenterLine = Nothing
End Sub