Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
    Dim dblX As Double, dblY As Double, dblZ As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    Dim cKPTyp As SolidEdgeConstants.KeyPointType
    Dim cHndTyp As SolidEdgeConstants.HandleType
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
    'Set the DatumReference to "A"
    objDatumTarget.DatumReference = "A"
    'Add a vertex at the end
    Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0)
    'Set the Leader line to true
    objDatumTarget.Leader = True
    'Set the BreakLine status to true
    objDatumTarget.BreakLine = True
    'Get the Key Point of the DatumTarget
    Call objDatumTarget.GetKeyPoint(Index:=1, x:=dblX, y:=dblY, z:=dblZ, _
                                    KeyPointType:=cKPTyp, HandleType:=cHndTyp)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
End Sub