Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfile As SolidEdgePart.Profile
Dim objL1 As SolidEdgeFrameworkSupport.Line2d
Dim objL2 As SolidEdgeFrameworkSupport.Line2d
Dim objD1 As SolidEdgeFrameworkSupport.Dimension
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
On Error GoTo 0
' Create a Profile and 2 line objects in it
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1))
Set objL1 = objProfile.Lines2d.AddBy2Points(x1:=0.05, y1:=0.05, x2:=0.03, y2:=0.03)
Set objL2 = objProfile.Lines2d.AddBy2Points(x1:=-0.05, y1:=-0.05, x2:=-0.03, y2:=-0.03)
' Create a Dimension object
Set objD1 = objProfile.Dimensions.AddAngleBetweenObjects(ele1:=objL1, x1:=0.05, _
y1:=0.05, z1:=0, keyPoint1:=True, ele2:=objL2, x2:=-0.03, _
y2:=-0.03, z2:=0, keyPoint2:=True)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfile = Nothing
Set objL1 = Nothing
Set objL2 = Nothing
Set objD1 = Nothing
End Sub