Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objC1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objD1 As SolidEdgeFrameworkSupport.Dimension
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create a Circle object in the Profile
    Set objC1 = objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
    ' Create a Dimension object
    Set objD1 = objProfile.Dimensions.AddRadius(Object:=objC1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objC1 = Nothing
    Set objD1 = Nothing
End Sub