Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objC1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objC2 As SolidEdgeFrameworkSupport.Circle2d
    Dim objDimns As SolidEdgeFrameworkSupport.Dimensions
    Dim objDim1 As SolidEdgeFrameworkSupport.Dimension
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    ' Create 2 Circle2d objects in the Profile
    Set objC1 = objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
    Set objC2 = objProfile.Circles2d.AddByCenterRadius(x:=0.02, y:=0.02, Radius:=0.01)
    ' Create a Dimension object
    Set objDimns = objProfile.Dimensions
    Set objDim1 = objDimns.AddSymmetricalDiameter(Object1:=objC1, x1:=0, y1:=0, _
                                                  z1:=0, keyPoint1:=True, object2:=objC2, x2:=0.02, _
                                                  y2:=0.02, z2:=0, keyPoint2:=True)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objC1 = Nothing
    Set objC2 = Nothing
    Set objDimns = Nothing
    Set objDim1 = Nothing
End Sub