Solid Edge FrameworkSupport Type Library
CropRight Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
SmartFrame2dStyle Object
: CropRight Property
Description
Sets and returns the distance from the origin of the referenced object to the right side of the frame or view.
Property type
Read-write property
Syntax
Visual Basic
Public Property CropRight As Double
Remarks
Specified in container units
See Also
SmartFrame2dStyle Object
|
SmartFrame2dStyle Members
Send comments
on this topic.