Solid Edge FrameworkSupport Type Library
Rotation Property
Description
For OLE objects, specifies the angle at which the object is rotated along its major axis. For hatch lines, sets and returns the rotation angle used to display hatch lines.
Property type
Read-write property
Syntax
Visual Basic
Public Property Rotation As Double
See Also

SmartFrame2dStyle Object  | SmartFrame2dStyle Members

Send comments on this topic.