Solid Edge Geometry Type Library
Edges Property
Description
Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Property type
Read-only property
Syntax
Visual Basic
Public Property Edges As Object
Remarks
The result of the Edges property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. By default, the Edges property returns all edges for the object. The topology collection can be restricted to a specified type of edge by supplying a value (from the FeatureTopologyQueryTypeConstants constant set) for the EdgeType argument for the feature objects only. For example, this property can be set to return all ellipse edges, straight edges, and so forth.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objEdges As Object
    Dim objBody As solidedgegeometry.Body
    Dim objVertex1 As solidedgegeometry.Vertex
    Dim objFaces As Object
    Const TESTFILE = "T:\vbtests\testcases\Vertices.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Model object
    Set objBody = objDoc.Models(1).Body
    ' Get the Faces collection
    Set objFaces = objBody.Faces(FaceType:=igQueryAll)
    ' Get a Vertex
    Set objVertex1 = objFaces(1).Vertices(1)
    ' Get the Edges property of Vertex
    Set objEdges = objVertex1.Edges
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEdges = Nothing
    Set objFaces = Nothing
    Set objVertex1 = Nothing
    Set objBody = Nothing
End Sub
See Also

Vertex Object  | Vertex Members

Send comments on this topic.